Answers

Without considering the effect of the other cast-in channel? Based on eota there should be factor to reduce the concrete cone resistance due to the effect of the neighboring anchors. Using the centerline of the anchor leg to the edge of the concrete member should only be considered if the anchor is not inside the "scrn" distance. If the distance, cs and cp, between my channel is more than on the table on page 14/36 can I consider centerline of the anchor leg to the edge of the concrete member as the edge distance?