Continuing Education Webinars


51:44

Gain a basic understanding of how to help protect structural steel in buildings through effective use of fireproofing systems.

There are various ways to protect exposed structural steel in the event of a fire, whether in an airport, shopping mall, or in a commercial building. This presentation will provide an overview of different methods of steel protection with a focus on…

7 chapters
1 PDH
56:19

Gain a basic understanding of how facade systems work in practice including attachment mechanisms, fire barrier & building code requirements.

A building’s facade can be one of its most striking features. Yet, behind the scenes multiple components are necessary to ensure the façade is safe and enduring. This course provides an overview of some of the necessary elements for successful fa…

6 chapters
1 PDH
55:25

Learn what architects can do to help ensure the interior wall performance is achieved on the concrete deck.

Multiple jobsite conditions can reduce the performance of interior walls and create problems for designers, owners, and building occupants. Learn what architects can do to overcome these challenges and help ensure their design intent transitions from…

4 chapters
1 PDH
57:58

Gain a basic understanding the means and methods for evaluating anchor systems, including hand calculations, load tables, and anchor design software.

There are various means and methods to approach anchoring application calculations. The purpose of this presentation is to provide an overview of these means and methods, which include hand calculations, load tables, and anchor design software. The p…

4 chapters
1 PDH
55:33

Gain a basic understanding of power actuated technology (PAF), including codes, standards and approvals with which the products must comply.

In order to convey this message effectively, the basics of the technology will be summarized, such as the way the tool works, safety standards to help to ensure user safety, and specific fastener characteristics which have been developed to advance t…

8 chapters
1 PDH
57:44

Gain insights on the design of reinforcing bars using qualified adhesive anchor systems.

This presentation will explain how reinforcing bars can be designed in accordance with the development and splice provisions of the American Concrete Institute ACI 318, "Building Code Requirements for Structural Concrete", and post-installed using an…

6 chapters
1 PDH
58:23

Cast-in anchor channel systems can now be designed according to International Building Code.

With the recent introduction of the ICC-ES Acceptance Criteria AC232, cast-in anchor channel systems can now be designed with recognition under the International Building Code. This presentation will explain the provisions given in AC232 for designin…

7 chapters
1 PDH
55:27

Get an introductory overview of the adhesive and mechanical anchor market.

This presentation will provide an introductory overview of the adhesive and mechanical anchor market, including the fundamental principles of anchor theory, which includes applications and design basis. Various types of anchors, including product spe…

7 chapters
1 PDH
58:19

Recent revisions enabled an adhesive system to be approved for post-installing reinforcing bars.

Recent revisions to the ICC-ES Acceptance Criteria for Post-Installed Adhesive Anchors in Concrete Elements (AC308) have made it possible for an adhesive system to be approved for post-installing reinforcing bars per the development and splice provis…

5 chapters
1 PDH