Expert Advice


Robin Lee
at 18 Apr 2018, 7:56 am

The client is adding new equipment. Typically they use Hilti HIT-V threaded rod to anchor this new equipment to the existing 6" plus (18" in this application) concrete floor. In this case, the bolt hole location is located at the constructi…

1 vote
20 views
1 answer
E_CE
at 17 Apr 2018, 4:44 am

I would just like to ask the implication of having undersized hole. If we have N28 rebar but have installed diameter 32mm hole (hilti hole requirement for N28 is 35mm), would it be acceptable?

0 votes
34 views
1 answer
Azat Khuzin
at 30 Mar 2018, 2:06 am

Какие анкера практичнее применять в кирпичной кладке для вспомогательных конструкций с небольшими нагрузками? Есть ли готовые решения?…

0 votes
68 views
2 answers